Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Can the Square D QED-2/Speed-D switchboard be wall-mounted instead of floor mounted?

Issue:

Wall Mount Conversion of QED-2/Speed-D Switchboard.

Product Line:

LV QED-2 switchboards.

Environment:

QED-2, Speed D.

Cause:

Customer would like to have their Square D QED-2/Speed-D switchboard Wall Mount not Floor Mount.

Resolution:

No. Every switchboard to be ANSI/NEMA compliant must be floor mounted. It must be screwed to the floor. It also needs a minimum space of 13mm 1/2 in between the wall and the back of the QED for adequate ventilation. Please consult clearances required for installation of a QED Switchboard on FA281846.