Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the capacitance value of each section of the voltage divider connected to the VPIS of a RM6 Gas Insulated Switchgear and Can this capacitive voltage divider in the switchgear work as a coupling device for PLCC Technology?

Issue:

Knowing the capacitance value of the voltage divider connected to the VPIS of a RM6 GIS.

Product Line:

RM6 Gas Insulated Switchgear

Environment:

RM6, GIS.

Cause:

Customer wants to know if the capacitive voltage divider in their switchgear can work as a coupling device for the PLCC technology as the Capacitive Voltage Transformer's principles.

Resolution:

The capacitance value of each section is between 30 to 35 pF. However, VPIS (Voltage Presence Indicating Systems for MV Switchgear) is not validated with PLCC, it has never been tested.