Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the catalog number of replacement neutral bonding provisions for 125 and 250 A NF panelboard?

Issue:

To replace existing standard neutral bonding provisions on a 125 and 250 A NF interior.

Product Line:

Panelboard.

Environment:

NF, 125A, 250A panel board interior.

Resolution:

80113-675-50 is the part number for 125 and 250 A neutral bonding provisions for NF Panelboards. Includes lugs and required screws. Find more replacement parts for NF Panelboards in our 1670DB0802 Data Bulletin.