Nuestras marcas

Impact-Company-Logo-English Black-01-177x54

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
What is the difference between QOU215 and QOU215H?

Issue:

What is the difference between QOU215 and QOU215H?

Product Line:

QO/QOB, QOU circuit breakers

Answer:

The QOU breakers are rated 120/240 Vac, which means the line to ground voltage cannot exceed 120 Vac. The QOU-H is rated 240 Vac, which means the line to ground voltage can be as high as 240 Vac.