Nuestras marcas

Bienvenido(a) al sitio web para México de Schneider Electric

Te damos la bienvenida a nuestro sitio web para México.
		
¿Cómo podemos ayudarte hoy?
Why Can’t I Link the M580 Controller to the Edge I/O NTS DTM in Control Expert v16?

Issue:

When attempting to integrate the Edge I/O NTS DTM with an M580 controller in Schneider Electric’s Control Expert v16, the link fails during DTM configuration.

Error message when trying to add Edge IO NTS DTM

Cause:

  • The firmware version of the Edge I/O device is incompatible with Control Expert v16.
  • The required minimum firmware version is V4.40 or higher for successful integration.
  • Network security tools (e.g., Zscaler) or incorrect IP settings may block communication.

Solution:

Verify Firmware Version:

  • Ensure the Edge I/O device firmware is V4.40 or later.
  • If not, update the firmware using Schneider Electric’s official firmware upgrade procedure.

Update DTM Catalog:

  • Make sure the latest DTM library for Edge I/O is installed in Control Expert v16.
  • Restart Control Expert after updating the catalog.

Test Communication:

  • After applying the above steps, reattempt linking the Edge I/O NTS DTM to the M580 controller.
  • Validate by performing a parameter read/write test.