Issue:
The date code is not visible on the box label or the interior label.
Product Line:
Homeline Load Centers
Resolution:
For some part numbers, the date code is not printed directly on the interior and box labels. Instead, it is incorporated into a QR code applied during the manufacturing process. These QR codes contain a serial number composed of the date code and a sequential number. One QR code is placed in the interior, and the other QR is applied to the end pack label. Additionally, another date code label is placed to the box of the panel.