Issue:
Need to know if RCTV connectors can be adapted to be RCTH.
Product Line:
Masterpact MTZ, Masterpact NW
Resolution:
Yes, RCTV connectors can be rotated 90° to be RCTH. They are the same connectors, simply installed in a different orientation, allowing them to be positioned vertically (RCTV) or horizontally (RCTH) without any restrictions.
For more details, please refer to Data Bulletin 48049-219-03, which confirms that the same rear connector kits are used for both RCTV and RCTH.