{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV212 communicate Profibus?

Article available in these languages: Spanish

Issue:
ATV212 Profibus communication

Product Line:
ATV212
S-Flex enclosed ATV212

Environment:
All models and serial numbers

Cause:
None

Resolution:
Profibus is not offered as a communication option.
There are several third party companies such as "Anybus" that may be able to provide a gateway option from Profibus to one of the  ATV212 integrated protocols (Modbus, BACnet, Metasys N2, or Siemens P1).

Schneider Electric Nigeria