Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find documentation for Power Monitoring Expert 7.2 (PME 7.2)?
Issue
PME 7.2 Documentation

Product Line
Power Monitoring Expert 7.2 (PME 7.2)

Environment
Documentation

Resolution
For general information visit the PME 7.2 Schneider Electric Site at the following link:
https://www.se.com/ww/en/product-range-presentation/61280-struxureware-power-monitoring-expert-7#tabs-top

The following documents are available on the Schneider Electric Site:
StruxureWare Power Monitoring Expert 7.2.2 What's New - EN
StruxureWare Power Monitoring Expert 7.2 Installation Guide- EN
StruxureWare Power Monitoring Expert 7.2 User Guide - EN
StruxureWare Power Monitoring Expert 7.2 Functions and Characteristics

The StruxureWare Power Monitoring Expert 7.2.2 System Design Guide is attached below.

To download PME 7.2 SP2, refer to article FA230563 .
To download PME 7.2 Cumulative Update 2, refer to article FA240221 .

Schneider Electric Nigeria

Attachment(s)
PME 7.2.2 System Design Guide.pdf [1.55 MB]