Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the PM8000 series meter's front display show Displacement Power Factor?

Issue
Can the PM8000 series meter's front display show Displacement Power Factor?

Product Line
PowerLogic PM8000 series meter

Environment
Meter front panel readings

Resolution
The PM8000 series meter's front screen shows True Power Factor.
One of the default arithmetic modules in the meter provides the displacement power factor. The details can be found in this KB article, How to view displacement power factor in advanced ION architecture meters? .

By creating a custom display screen, the Displacement Power Factor can be selected and viewed.  Step-by-step instructions for creating custom screens on the PM8000 are detailed at Video: PowerLogic PM8000 series meter custom screens