EM4800 - How to change the logging interval for energy
Issue
Customer can’t change the logging interval for Energy
Product Line
EM4000 Series
Environment
EM4800 Configuration Tool
Cause
Some customers’ applications may need to change the logging interval for Energy.
Resolution
1. Connect to the meter using the EM4800 Configuration Tool.
2. In the Report section, open the Reporting Schedule tab.
3. Change the interval setting as desired:
4. Unit > Save to save the configuration.
5. Unit > Send to send changes to the meter.
Links
- PowerLogic EM4800 Configuration Tool download
- E4800, EM4800, EM4000 Tenant Meter Guides / Manuals / Instructions
Released for: Schneider Electric Nigeria