{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

What is the difference between DC Braking and Dynamic Braking?

DC Injection Braking is used to hold a load in position after the motor has stopped. This is done by injecting DC voltage into the motor creating holding torque. DC braking is not meant when a large...

What is the difference between In-line and Inside Delta Soft Starter...

The Altistart 48 connected in the motor supply line The motor connection depends on the supply voltage, which in this example is a star connection. The motor connection depends on the supply voltage,...

what is the difference between PTC & PT100 their function and connecting...

- PT100 is an RTD (Resistance Temperature Probe) made of Platinum metal which has a resistance value of 100 ohms at zero degrees celsius. - PTC (Positive Temperature Coefficient) and NTC (Negative...

How to share variables between Machine Expert (EME) PLC and Operator...

Issue: The M241 / M251 / M262 PLC is not communicating with HMIST6 programmed with EcoStruxure Operator Terminal Expert. Product Line: SoMachine, EcoStruxure Machine Expert, EcoStruxure Operator...

What are the values of earth loop impedance for Compact NSX MCCBs and...

For earth loop impedance, we can provide the method and the customer calculates it according to his need. Our colleagues of Schneider UK have made Zs calculations for Compact NS and NSX, see the...

Video: How do you wire the ATS22 with S6U suffix, for 2-wire control?

Issue: Wiring the ATS22 with S6U suffix, for 2-wire control. . Product Line : Altistart 22 Environment: All Altistart 22's ending with S6U suffix (120V) Cause: Basic wiring examples Resolution :...

Can we control circuit breaker through wifi?

We can only control On and OFF through isc (which is connected to router Which has wifi ) please check more information through the link below...

what is the Installation guide for RCCB for 3P without neutral ?

Please refer the attached document connection in 3P RCCB. You can follow the same document for connection in three-Phase without neutral. >> If you are using Acti9 range RCCB, You don't...

Show more

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
Show more

Learn more through our Generic Knowledge FAQsGeneral Knowledge

What is meant by Symmetrical and Asymmetrical breaking currents?

issue: Customer wants to know the value of the symmetrical and asymmetrical breaking current of the circuit breaker and what do they mean. Environment: Circuit Breaker Resolution: - Symmetrical...

In a 3 phase system, why does the meter still show voltage reading on one...

Issue: Testing phase loss on a meter doesn't result in a null voltage reading. Environmnet: EasyLogic Series Power Meters PowerLogic Series Power Meters Resolution: The voltage seen is what we...

What is the selection criterion of Circuit Breakers for the Capacitor bank...

The selection should be done after derating the Circuit Breaker taking into consideration voltage variation and capacitors tolerances that could increase nominal current up to 1.5In. The Derating...