{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

What is the difference between the GV2P and the GV2L

The GV2P breakers have thermal and magnetic protection, GV2L Breakers have magnetic only.

What are the Rated short-circuit making capacity (Icm) and Rated...

Rated short-circuit making capacity (Icm) and Rated short-time withstand current (Icw) values for Compact NSX Switch-disconnectors can be found in Compact NSX Catalogue . Icw and Icm values are...

How do I access Proface panel GP-4502WW in GP-Pro EX version 4?

The user manual for GP-Pro EX describes the following: You could be using GP-Pro EX software version 4.09 and still GP-4502WW model may not be available/displayed as an option. In that case, please...

When selecting bus bar for GV2, or U-line starters, what does "pitch" mean?

Issue: When selecting bus bar for GV2 or U-line starters what does "pitch " mean? Product Line: IEC starters Environment: GV2 and U-line starters Cause: Product description and installation...

What are the main differences between Masterpact MTZ and Masterpact NT/NW?

MaterPact MTZ follows the same footprint as of NT/NW. However, it uses Micrologic X which is only compatible with MTZ. MTZ is an advanced/modern ACB which is future ready as well as EcoStruxure...

What is the alternative part number for XSPH08362?

The replacement part number is XS4P18AB120 See attached data sheet for details.

What is the part code for a 3 Phase 32A 30mA RCBO?

We do not offer a single 3 Pole 32 Amps 30mA RCBO. You can use 3 Pole 32 Amps iC60 MCB and connect it with the 3 Pole Add-on Vigi Module "A9V02763" (comes with the neutral tail to be...

Can the Domae Earth leakage RCBO DOM12530 be Top or Bottom Fed?

Yes, the feed can be supplied to the top or bottom of the Domae RCBO's.

Show more

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
Show more

Learn more through our Generic Knowledge FAQsGeneral Knowledge

Why choose Type B RCD for 3 Phase Variable Speed Drives?

For the 3 Phase Variable Speed Drives, the RCD type B or type B-Si is particularly suitable. It protects against fault currents with DC offset, which is true for three-phase power converters. In...

What are the effects of dV/dt on a Motor when using a VSD?

As there is an impedance mismatch at the termination of the motor cable to the motor, there will be a reflected wave which travels back along the motor cable causing overvoltage’s. Overvoltage’s on...

How do I access the Tools Page in eDLT

Press and hold down the bottom left button, whilst continuing to hold then double press the top right button. Please note that access to the Tools Page can be disabled using C-Bus Toolkit software.

How to lodge warranty claims to Schneider Electric Australia for Schneider...

Go to the SE Solar - Get Support website https://solar.schneider-electric.com/netsuite/ Fill in all mandatory fields, upload a scan of proof of purchase (customer invoice), supporting photos, single...

What is Modbus and How does it work?

What is Modbus? Modbus is a serial communication protocol developed by Modicon published by Modicon® in 1979 for use with its programmable logic controllers (PLCs). In simple terms, it is a method...

What are the ranges of the Square D Circuit Breakers?

Material Description Comment Direct Replacement QO106EC10 MINIATURE CIRCUIT BREAKER 240V 6A Discontinued no replacement QO110EC10 QOvs 1P 10A 10kA Type C Direct Replacement QO110VSC10 QO116EC10 QOvs...

Can I use a 15A socket with a 10A plug?

Yes, a 15A socket with a 10A plug will fit.

ETSNZ - What is the material used in making the fire barrier in a length...

The material used is called Vermicullite.

Show more