{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

What does the 's' on the Power Meter Accuracy class 0.2s & 0.5s mean?

It refers to the accuracy of the meter. A 0.2s meter has a much higher accuracy as below. Since Accuracy depends on the load of the system, IEC/AS have developed different standards to define...

How hot can circuit breakers get? What is the temperature of a molded...

Issue: What is the temperature of a molded case breaker? Product Line: Circuit Breakers Resolution: The acceptable operating temperature of a circuit breaker is defined by UL in the UL489 standard...

What is the replacement for the LA2-D22-A65

It will be the LADT2 and is only compatible with the TeSys D and TeSys F range.

What are the main differences between Micrologic X and Micrologic 2/5/6/7 ?

Micrologic X control unit is designed and dedicated for MTZ range only. It is an advanced control unit and comes embedded with features such as Bluetooth, NFC and a USB-C port whereas Micrologic...

How Can I Change a Wiser Mechanism from Zigbee to Bluetooth

To swap a Zigbee enabled switch to Bluetooth, press the switch 4 times and hold on the 4th press for 20+ seconds. When holding the button in at the 10 second mark a slow flashing red led should be...

What is a current limiting circuit breaker?

Issue: What is a current limiting circuit breaker? Product Line: Molded Case Breaker, Powerpact Resolution: A current limiting circuit breaker is one that has been certified by UL to limit the...

What is the complete RJ45 connector pinout for ATV320?

The complete pinout, Pin 1 = CAN_H Pin 2 = CAN_L Pin 3 = CAN_GND Pin 4 = DI Modbus Signal Pin 5 = DO Modbus Signal Pin 6 - Not connected Pin 7 = VP, 10Vdc Pin 8 = Common The CANopen signals on the...

How can I connect SoMove to an Altivar Process drive via Ethernet TCP/IP...

Issue: Connecting SoMove to the VFD using the Ethernet network connection. Product Line: ATV61 ATV71 ATV630 ATV930 ATV320 ATV340 ATV32 Environment: Ethernet IP or Profinet option installed. VW3A3316,...

Show more

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
Show more

Learn more through our Generic Knowledge FAQsGeneral Knowledge

Why choose Type B RCD for 3 Phase Variable Speed Drives?

For the 3 Phase Variable Speed Drives, the RCD type B or type B-Si is particularly suitable. It protects against fault currents with DC offset, which is true for three-phase power converters. In...

How to lodge warranty claims to Schneider Electric Australia for Schneider...

Go to the SE Solar - Get Support website https://solar.schneider-electric.com/netsuite/ Fill in all mandatory fields, upload a scan of proof of purchase (customer invoice), supporting photos, single...

What are the effects of dV/dt on a Motor when using a VSD?

As there is an impedance mismatch at the termination of the motor cable to the motor, there will be a reflected wave which travels back along the motor cable causing overvoltage’s. Overvoltage’s on...

How do I access the Tools Page in eDLT

Press and hold down the bottom left button, whilst continuing to hold then double press the top right button. Please note that access to the Tools Page can be disabled using C-Bus Toolkit software.

What is Modbus and How does it work?

What is Modbus? Modbus is a serial communication protocol developed by Modicon published by Modicon® in 1979 for use with its programmable logic controllers (PLCs). In simple terms, it is a method...

What are the ranges of the Square D Circuit Breakers?

Material Description Comment Direct Replacement QO106EC10 MINIATURE CIRCUIT BREAKER 240V 6A Discontinued no replacement QO110EC10 QOvs 1P 10A 10kA Type C Direct Replacement QO110VSC10 QO116EC10 QOvs...

Can I use a 15A socket with a 10A plug?

Yes, a 15A socket with a 10A plug will fit.

ETSNZ - What is the material used in making the fire barrier in a length...

The material used is called Vermicullite.

Show more