Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the Altistart 48 require separate control power?
Issue:
Does the ATS48 require separate control power?

Product Line:
ATS48

Environment:
All

Resolution:
Yes, terminals CL1 and CL2 require 90 to 270 Vac, 50/60 Hz to supply control power.
It is common to use 120 VAC to supply power for the ATS48 control power.