Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a dynamic braking resistor be installed on an ATV212 or ATV21 drive?
Issue:
ATV212 (or ATV21) connection for a DB resistor

Product Line:
ATV21, ATV212

Environment:
All Models and Serial Numbers

Cause:
Installation question

Resolution:
No, you cannot put a braking resistor on an ATV21/212 drive. These drives are not designed to be installed with a braking resistor.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: