Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the baud rate switch settings for the Advantys STBNCO2212 CANopen NIM?

Issue:
How to set the baud rate on the Advantys STBNCO2212 CanOpen NIM.

Product line:
Advantys Configuration Software

Resolution:
When the lower switch is turned to any one of its baud rate positions, the baud rate is defined by the position on the upper switch. Only positions 0 through 7 are used to set the baud.
image

NOTE: The default baud in Flash memory for a new STBNCO2212 CANopen NIM is 1 Mbits/s.