Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to configure the drive so that when the f4 key is pressed it does nothing?

Issue: Is it possible to configure the drive so that when the f4 key is pressed it does nothing?

Product Line: ATv61 ATV71 VW3A1101

Environment: All

Cause: Unassigning the F4 button

Resolution: You can't completely unassign the F4 button.  If you assign the F4 key function to Not assigned, the F4 buttom will display quick and when pressed it will bring you to the quick menu.