Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the default TCP port number of the native Ethernet Port on M340 BMXP342020 processor.

Product:

M340

Answer:

The proprietary TCP port number for Modbus/TCP traffic for the M340 BMXP342020 processor's native ethernet port is 502.