Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the communications cable between the Twido minidin and Magelis HMISTU655/855 RJ45 port?

Issue:
Communications cable to use between the Twido mini din and Magelis HMISTU655/855 RJ45 port


Product Line:
Twido, HMISTU


Resolution:
The communications cable between the Twido PLC and the HMISTU655/855 is the XBTZ9780.