Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to associate the energies to the analog output of IOX extender module ?

Issue
End user would like to know if it is possible to associate the energies to the analog output of IOX extender module.

Product
PM8000 Series

Environment
Power Meter
PM8000 Series

Cause
Is it possible to associate the energies to the analog output of IOX extender module?

Resolution
Yes, the 3 energies (real, reactive and apparent) could be associated with analog output of IOX extender.