Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which fuses are used with the Enercept Meter and the Energy Meter Fuse pack?

Issue
Would like to know fuse class for fuses included in the energy meter fuse packs

Product Line
EMFP1
EMFP2
EMFP3

Environment
Installation

Resolution
The replacement fuses for the voltage fuse pack with the Enercept Meter or Energy Meter are 1/2 AMP Cooper, Bussmann, FNQ-R-1/2, CC-Tron, Class CC, Slow Blow.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre