Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are conduit kits available for the ATS22 series soft starters?

Issue:
Conduit kits availability for the ATS22 series.

Product Line:
Altistart 22


Resolution:
Conduit kits are not available for the ATS22 series starter.  To bring them up to a particular NEMA rating, they will need to be installed in a properly sized NEMA rated enclosure.  Schneider Electric does offer a line of Enclosed ATS22 starters that can be built to order.  Check with your local distributor for Enclosed ATS22 Soft Starter options.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)