Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
MC_touchProbe Window function is not possible when touch probe is connected in LXM32
When the probe is connected in LXM32, the windows function MC_TouchProbe is not permitted. Our work around is when axis is in window position, the MC_TouchProbe function is active. When axis is out of windows position, the MC_TouchProbe function is inactive.

Schneider Electric Saudi Arabia

Attachment(s)
MC_TouchProbe.pdf [107.05 KB]