Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I program an ATV12 for a preset speed?

Article available in these languages: Spanish

Issue:
Preset speeds set up for an ATV12.

Product Line:
ATV12

Environment:
All

Cause:
Installation / Setup

Resolution:
Set desired logic input (LIx) to  PS2 in the FUN menu under PSS (Preset Speed) , then set SPx = desired speed. Note: you must be in terminal mode operation and low speed (LSP) will be the 1st  preset speed.