Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ATS22 soft starters come with built in overload protection?
Issue:
Does the ATS22 soft starters come with built in overload protection?

Product Line:
Altistart ATS22

Environment:
All

Cause:
Needs to know if the ATS22 soft starter has a built in overload protection

Resolution:
Yes, the ATS22 soft starters have built in overload protection.
The default motor thermal protection is IEC class 10.
You can adjust this value in the programming in the SEt menu.
Parameter tHP