Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the ATS48 remote keypad display mounting kit, and what is included in it?

Article available in these languages: Spanish

Issue:
Is there a remote keypad for the ATS48?

Product Line:
ATS48

Environment:
All

Cause:
Remote keypad required

Resolution:
Part number VW3G48101 is the kit, and includes:
Keypad with 3–character 7–segment display,
IP65 cover and seal,
Mounting screws,
3 meter cable to connect keypad display to Altistart 48.

Note:  The kit is not rated for outdoor use.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)