Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there any Ethernet/IP Client available in SoMachine or Machine Expert?
Starting with SoMachine  version 4.1 SP2, an EtherNet/IP Client device for TM251MESE controllers is available. TM251MESC controllers do not have this feature available in SoMachine or Machine Expert 1.2 or 2.x

Starting with SoMachine version 4.2, an Ethernet/IP Client device for TM241CE controllers is also available. TM241CEC** controllers do not have this feature available in SoMachine version 4.2 but starting with SoMachine version 4.3 it is is available.

All M262 controllers which were introduced with Machine Expert have the Ethernet/IP Client functionality.

Note: SoMachine software is now called Machine Expert. The last version of SoMachine was 4.3.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre