Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ENM Monitoring and Diagnostics pages display "[Invalid Date]" for timestamps

Issue

The Event Notification Module (ENM) Monitoring and Diagnostics pages display [Invalid Date] in timestamp columns instead of the actual timestamp.

Product Line

ENM 8.3.x

Environment

PowerSCADA Expert 8.1

Power Monitoring Expert 8.1

Cause

Some Windows locales use special characters for AM/PM notation (e.g., Italian [Switzerland], Chinese [Singapore]). When Windows is configured to use one of these locales, ENM cannot properly format timestamps, resulting in [Invalid Date].

Resolution

Change the Windows locale to one that uses standard AM/PM characters.
Examples:

  • Italian (Italy)
  • Chinese (China)

Steps:

  1. Open Control Panel → Region and Language.
  2. Change the locale to a supported setting.
  3. Restart ENM services if necessary.

Notes

  • This issue applies only to ENM 8.x and PME 8.1.
  • Newer versions of PME and ENM have resolved this locale parsing issue.

Recommendation

If you are using an older version of PME or ENM, upgrading to the latest version is strongly recommended. Upgrading provides better compatibility, improved security, and fixes for known issues.
For upgrade assistance, contact: pmo-psup@se.com.