Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you set up the ATV312 for auto manual control?
Issue:
ATV312 setup for auto, manual control

Product Line:
ATV312

Environment:
All

Cause:
Want to set up an 3 position switch for HOA control.

Resolution:

CTL menu
Fr1 = Ai1
Fr2 = AI3
RFC = LI3

You will need to also turn off preset speeds:
FUN menu
PSS
PS4 set to no
PS2 set to no

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre