Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to setup a run permissive on a Altivar Process Drive.
Issue:
Altivar Process Drive permissive run set up.

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Resolution:
To setup a run permissive use Freewheel Stop Assignment
[Complete settings] [Generic functions] [Stop configuration] [Freewheel stop ass.] nSt