Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which reference of power contact to select in Harmony range for a direct assembly on PCB? PCB drilling dimensions?
It is possible to mount power contact blocks and light modules (led and Ba9s) directly on PCB selecting the following references:
Contact blocs: ZBE101A and ZBE102A
Led modules: ZBVB*A
Ba9s block: ZBV6A

Another option for direct mounting of contact blocks and led blocks is to use contact blocks ZBE701, ZBE702 and led blocks ZBVB*7: see attachment (catalogue extract)
but these contact blocs are not power contact

Schneider Electric Saudi Arabia

Attachment(s)
ZBE---A drilling dimensions.pdf [20.12 KB]
ZBE blocks direct mounting.pdf [31.05 KB]
ZBE-7 mounted on PCB.pdf [93.29 KB]