Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I correct my Unity v11.1 FBD block and font sizes?
Block size used when exporting a project is done according to Windows zoom setting.
After export on a given machine/PC, if you import on another machine/PC with a different Windows zoom setting, the user will see blocks and fonts bigger or smaller,
depending on the settings of each machine/PC.

Resolution:
To get the same block, size please change the Windows setting and for the font size, also modified the Windows setting to match the original machine/PC settings.