Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is a start check warning (code 46) on a Tesys T LTMR product?
Issue:
Customer is receiving error 46 Start Check on their Tesys T product.

Product Line:
TeSys T - LTMR

Environment:
US Product

Cause:
Product Specification

Resolution:
Start command check (Error 46) signifies that current is not detected after a delay of 1 second after a start command.  The unit must see a current equal to or more than 10% of FLC minimum.  If the unit is being tested without a motor load, ensure that a current of more than 10% FLC minimum is being passed through the internal CT windows of the device.