Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many option cards can you add to the ATV320?
Issue:
ATV320 usage of option cards

Product line:
Altivar 320, ATV320

Environment:
All

Cause:
Installation

Resolution:
Altivar Machine ATV320 drives are designed for use with option modules according to machine and application requirements. One option module can be used with an Altivar Machine ATV320 at a time. The option modules are compatible with all Altivar Machine ATV320 drives.

NOTE - The VW3A3600 option module adapter is required to connect an option module to compact-style Altivar Machine ATV320 drives (part numbers that end with a "C" , ATV320...C).