Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
On Ativars ATV61, ATV71, can I use PTC connected to LI6 and external 24V for logic inputs at the same time?
Yes it is possible. Wiring in attachment
Do not forget to set SW2 switch = PTC
To enable PTC monitoring, in Drive menu - Fault management - LI6 as PTC = (anything different from "no")

Schneider Electric Saudi Arabia

Attachment(s)
Pict_scheme.jpg [75.27 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre