Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which motor control type should be used for a pump or fan application on an ATV630 Drive?
Issue:
On an ATV630 what motor control type should be used for a pump or fan application?

Product Line:
Altivar 630

Environment:
Pump or fan applications

Cause:
Basic programming

Resolution:
U/F VC Quad should be used for pumps and fans.

motor control type
In some applications that require higher starting torque other motor control types may be required.

Please see the ATV600 Programming Manual for additional details:
https://www.se.com/ww/en/download/document/EAV64318/

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre