Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the power consumption rating (watts) for the control voltage, of the ATS48?
Issue:
Looking for the power consumption rating (watts) for the control voltage, of the ATS48?

Product Line:
Altistart 48

Environment:
All models and serial numbers

Cause:
Documentation

Resolution:
ATS48D17Y to ATS48C17Y- 30 W
ATS48C21Y to ATS48C32Y- 50 W
ATS48C41Y to ATS48M12Y- 80 W