Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In EBO server Modbus TCP network/device basic properties tab, what does "Multiple queries" mean?

In EcoStruxure Building Operation "EBO" Server Modbus TCP network/device basic properties, "Multiple queries" means that a number of queries will be sent out at the same time. The system will wait for those responses. If this option is disabled, the system will send one query and the wait for a response.  "Multiple queries" is only supported on some Modbus devices, so make sure that the integrated Modbus device supports this option before enabling it. "Multi queries" can be enabled/disabled at the Modbus TCP network or device level.
Modbus multiple queries configuration

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre