Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the fuse type used in the GS2 Disconnect Switches?
Issue:
Need to know the fuse type for the GS2 Disconnect.

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
GS2 Fusible Disconnect Switches

Resolution:
GS2 rated from 30-60A will use a Cartridge Type fuse.  Switches from 100-800A will use a Blade Type fuse.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre