Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unity Pro 13 Registration Wizard tool location

Issue
After I've installed Unity Pro v13.x, where do I find the Registration Wizard tool?

Product Line
Unity Pro 13.x for Modicon PLC configuration software for Windows

Environment
Configuration software installed in Windows 7 or above.

Resolution
If you are running on Windows 7 or 8, the icon may be found in the Start Bar in the folder path with a light blue icon:
Schneider Electric -> SoCollaborative -> Unity Pro -> Registration Tool

If you're running Windows 10, you may have difficulty finding the Registration Wizard from the Start Bar.
The file location is:
<Unity Pro InstallFolder>\RegUpXL\RegistrationWizard.exe

If you've installed in the default location, it would be the direct path:
C:\Program Files (x86)\Schneider Electric\Unity Pro\RegUpXL\RegistrationWizard.exe

Note: EcoStruxure Control Expert v14.0 and above uses the newer shared Schneider Electric License Manager Tool.
It is located in the default install location:
C:\Program Files (x86)\Schneider Electric\License Manager\LicenseManager.exe

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)