Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Citect support CtAPI protocol?
Yes, CtAPI (Citect SCADA API) allows access to Citect SCADA I/O variable tags via a DLL interface. This allows 3rd party developers to create applications in C ( or other languages) to read and write to the I/O Devices, to use data query and to call Cicode functions.
There is no additional license required to use CtAPI.