Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you use Rogowski coil input for PM8000 series meters?
Issue:
Can you use Rogowski coil input for PM8000 series meters?

Environment:
PowerLogic PM8000 series meters

Resolution:
No. Rogowski current transformers are only compatible with the EM/iEM series, like:
PowerLogic EM3500 - EM3555A EM3502A EM3560 EM3550A EM3560 EM3561A
PowerLogic EM4200 - EM4236 EM4235
cti9 iEM3000 - iEM3555 iEM3565.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre