Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Error when trying to download Machine Expert v2.0.x
Issue
Error when trying to download Machine Expert 2.0.x. Need to upgrade to new installer

Product Line
EcoStruxure Machine Expert

Environment
PLC Configuration Software - Logic Builder

Resolution
When Machine Expert v2.0 came out, a new software installer was released with it. The tool is called "Schneider Electric Software Installer" It allows for downloads of Machine Expert v2.0.x and lower.

Click here for Machine Expert download page

software