Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you read the digital input assignments over ethernet on the ATV61/71 Drives?


Issue:
Is it possible to read the digital Input assignment over ethernet for all inputs?

Product Line:
Altivar 61 Altivar 71 and Altivar Process Drive

Environment:
All

Cause:
Communications Inquiry

Resolution:
Yes, you can read Logic/Digital Input Assignments over the network.
See document attached for explanation.

Schneider Electric Saudi Arabia

Attachment(s)
Page 1.jpg [166.75 KB]
Page 2.jpg [167.61 KB]
Page 3.jpg [189.11 KB]