Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the minimum and maximum ohm values for braking resistors for the ATV930 drives?

Article available in these languages: Spanish

Issue:
Needs ohmic values for ATV930 braking resistors.

Product Line:
ATV930

Environment:
230V up to 75KW, 480V up to 310KW, 600V up to 75KW, 690V up to 90KW.

Cause:
None.

Resolution:
See the attached document showing Min. and Max. ohm values.

Schneider Electric Saudi Arabia

Attachment(s)
ATV900_Braking_IE04 600 Volt (1).pdf [412.75 KB]