Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to reduce motor noise when driven by an ATV320?

Article available in these languages: Japanese

Issue:
The motor is quite noisy while running

Product Line:
ATV320

Environment:
ATV320 all series

Cause:
ATV320 is creating too much motor noise.

Resolution:
Options include:

Set noise reduction (nrd) to yes.  This creates a random frequency modulation which helps prevent a resonance.
Conf > FuLL > drC- > nrd = YES

Increase the switching frequency (SFr).  This may also increase the heat generated by the drive.
Conf > FuLL > drC- > SFr: (there is a range between 2 to 16kHz depending on the drive size).

Consider mounting characteristics to a machine.  Use mechanical joints (silent block) between the motor and the frame of the machine. It will help to suppress low frequency vibrations.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre