Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why when using the Print function on Ecostruxure Machine Expert Basic v1.2 do I get a blank page in the POU section?

Issue:
Why when using the Print function on Ecostruxure Machine Expert Basic v1.2 do I get a blank page in the POU section?

POU in blank

Product Line:
Ecostruxure Machine Expert - Basic v1.2


Cause:
Unfortunately, there is a known anomaly in the software causing this issue, there is a new Service Pack available to fix this.


Resolution:

From v1.2 SP1 this software anomaly was mitigated, therefore, you should update to the said version or above.

Link to download the newest version: https://www.se.com/us/en/download/document/MachineExpertBasic_V1_2_SP1_P1/

Note: Unfortunately, you cannot downgrade a project to open it with an older version of EME-Basic. For instance, you cannot open an EME-Basic v1.2 project with EME-Basic v1.1

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre