Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an IHF or input overheating fault on the ATV680 enclosed drives?

Issue:

IHF or Internal overheating fault

Product Line:

ATV680 and ATV980 enclosed drives

Environment:

All

Cause:

AFE brick can be overheating or the drive ambient temperature is to high.

Resolution:

-Check Ambient temperature conditions

-Check to see if the heatsink is blocked.

-Look at the Drives thermal state the THDA setting

-Check the 48vdc cooling fan power supplies to see if they are powered up if the drive is powered on with a run command.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre