Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the TA1 -TA4 parameters in the ATV61/ATV71 drives?

Issue:
TA1 -TA4 parameters in the ATV61/ATV71 drives.

Product Line:

ATV61/ATV71 drives

Resolution:

TA1 (Rounding of the start of the ACC ramp) -Factory default is 10%

TA2 (Rounding of the end of the ACC ramp)-Factory default is 10%

TA3 (Rounding of the start of the DEC ramp)-Factory default is 10%

TA4 (Rounding of the end of the DEC ramp)-Factory default is 10%

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.